Skip to main content
Explorer II
September 10, 2024
Solved

Mono chrome display with STM32 Nucleo-144

  • September 10, 2024
  • 1 reply
  • 720 views

Hi,

I am looking for monochorme display which can be interfaced with STM32 Nucleo-144 board. I looked into TouchGFX but it supports colored display board with this STM32 Nucleo-144 board. 

Can you suggest any monochomre display based board here?

https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html

Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello @mdalal ,

    Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs .. 

    TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)

    SofLit_0-1725966430873.png

     


    @mdalal wrote:

    Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?


    There is no ready to use example STM32 Nucleo-144 board with a monochrome display.

    See also these threads:

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-configure-touchgfx-with-a-monochrome-lcd-on-fmc/td-p/583195

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/basic-touchgfx-project-with-monochrome-spi-e-paper-display/td-p/641466

     

    1 reply

    mƎALLEmAnswer
    Technical Moderator
    September 10, 2024

    Hello @mdalal ,

    Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs .. 

    TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)

    SofLit_0-1725966430873.png

     


    @mdalal wrote:

    Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?


    There is no ready to use example STM32 Nucleo-144 board with a monochrome display.

    See also these threads:

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-configure-touchgfx-with-a-monochrome-lcd-on-fmc/td-p/583195

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/basic-touchgfx-project-with-monochrome-spi-e-paper-display/td-p/641466