Most basic setup for SWD to work?
Hello, i need help with na stm32l031k6, I want to just start the processor and read it with an st-link v2, I have connected BOOT0 to GND(i haven't added a 10k resistor, but that shouldn't be the problem ), NRST with pull-up 1k to VDD, VDDA and VDD are connected together. From what I read online I can pass without the external crystal because there is an internal one. So when I connect the VDD to 3v3 on the st-link, the GND to the st-link GND, SWCLK to PA14, SWDIO to PA13 and the chip isn't recognized. I have ruled out an faulty st link because it recognizes a blue pill f103 board. Please tell me if I am forgetting something