mt25ql512abb in memory mapped mode not working
I am writing a custom driver for the mt25ql512abb as the one on STM's github doesnt work for my STM32L412KB, I have gotten reading, writing and erasing working but when I try enter memory mapped mode DQ[0-3] on the flash just goes high
Here is my function that im using, I am setting the XIP bit on the Volatile configuration register first (i have confirmed this is working) then I enter memory mapped mode, i have set the dummy cycles to 10 on the volatile and non-volatile configuration registers as well.
uint8_t CSP_QSPI_EnableMemoryMappedMode(void) {
QSPI_CommandTypeDef sCommand;
QSPI_MemoryMappedTypeDef sMemMappedCfg;
/* Enable Memory-Mapped mode-------------------------------------------------- */
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.AddressSize = QSPI_ADDRESS_32_BITS;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
sCommand.AddressMode = QSPI_ADDRESS_4_LINES;
sCommand.DataMode = QSPI_DATA_4_LINES;
sCommand.NbData = 0;
sCommand.Address = 0;
sCommand.Instruction = 0xeb;
sCommand.DummyCycles = 10;
sMemMappedCfg.TimeOutActivation = QSPI_TIMEOUT_COUNTER_DISABLE;
uint8_t config = 0xa3;
if(QSPI_WriteVCR(&config) != HAL_OK) {
return HAL_ERROR;
}
if (HAL_QSPI_MemoryMapped(&hqspi, &sCommand, &sMemMappedCfg) != HAL_OK) {
return HAL_ERROR;
}
return HAL_OK;
}
Here is my working read memory function
uint8_t CSP_QSPI_ReadMemory(uint8_t* buffer, uint32_t address, uint32_t buffer_size) {
QSPI_CommandTypeDef sCommand;
uint32_t end_addr, current_size, current_addr;
/* Calculation of the size between the write address and the end of the page */
current_addr = 0;
while (current_addr <= address) {
current_addr += MEMORY_PAGE_SIZE;
}
current_size = current_addr - address;
/* Check if the size of the data is less than the remaining place in the page */
if (current_size > buffer_size) {
current_size = buffer_size;
}
/* Initialize the adress variables */
current_addr = address;
end_addr = address + buffer_size;
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.AddressSize = QSPI_ADDRESS_32_BITS;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
sCommand.Instruction = 0xeb;
sCommand.AddressMode = QSPI_ADDRESS_4_LINES;
sCommand.DataMode = QSPI_DATA_4_LINES;
sCommand.NbData = buffer_size;
sCommand.Address = address;
sCommand.DummyCycles = 10;
/* Perform the write page by page */
do {
sCommand.Address = current_addr;
sCommand.NbData = current_size;
if (current_size == 0) {
return HAL_OK;
}
/* Configure the command */
if (HAL_QSPI_Command(&hqspi, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
return HAL_ERROR;
}
/* Transmission of the data */
if (HAL_QSPI_Receive(&hqspi, buffer, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
return HAL_ERROR;
}
/* Configure automatic polling mode to wait for end of program */
if (QSPI_AutoPollingMemReady(HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
return HAL_ERROR;
}
/* Update the address and size variables for next page programming */
current_addr += current_size;
buffer += current_size;
current_size =
((current_addr + MEMORY_PAGE_SIZE) > end_addr) ?
(end_addr - current_addr) : MEMORY_PAGE_SIZE;
} while (current_addr <= end_addr);
return HAL_OK;
}
any help would be great thanks