Skip to main content
Visitor II
October 13, 2025
Question

MT35XU02GCBA2G12-0AUT compatibility with STM32N6 XSPI?

  • October 13, 2025
  • 1 reply
  • 160 views

Hi everyone,
Has anyone interfaced the Micron MT35XU02GCBA2G12-0AUT (2 Gbit xccela Flash) with the STM32N6 XSPI controller?

I  would like to know if it works with the existing Macronix presets or needs custom XSPI settings.
Any working example or experience would help.

Thanks!

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 13, 2025

    Hello @GBA ;

     

    Could you please share the memory datasheet?

    To check whether a device is supported by the XSPI interface, you need to refer to memory datasheet and the STM32N6 reference manual and precisely the command format and order.

    The command format and order shared in the device datasheet must be aligned with the command format and order mentioned in the STM32 reference. 

     

    Thank you.

    Kaouthar