Multiple value for VECT_TAB_OFFSET on STM32H7
Hi all, we've been developing some applications using STM32H743BG since 2020 and only now we realized that value of VECT_TAB_OFFSET has been changed according the package used in STM32Cube. So, these are the differences between different Cube versions:
STM32Cube FW_H7 V1.9.0:
#define VECT_TAB_OFFSET 0x00000000UL /*!< Vector Table base offset field. This value must be a multiple of 0x200. */
STM32Cube FW_H7 V1.10.0:
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field. This value must be a multiple of 0x300. */
STM32Cube FW_H7 V1.11.1:
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field. This value must be a multiple of 0x400. */
So, my question is: what offset value should be used? Offset of 0x200, 0x300 or 0x400?
Where is possible to find this information on the available documentation?
Regards,
Tiago F. Borth