Need help with project - NUCLEO-F746ZG, NTP, Time Stamping Events
Hello! I am currently working on a project involving a NUCLEO-F746ZG board that is connected to a local NTP server and another board (let's call it X). My board needs to be synchronized with the NTP server and receive 3 pairs of timestamps from board X. These 3 pairs represent 3 time intervals during which my board must allow a signal to pass through it and reach board X. I can compare my board to a valve that lets water flow through a pipe at a specific time. My board should not introduce latencies greater than 1ms (I understand that NTP can achieve these performance levels), and because of this, I think synchronization with the NTP server should be done quite frequently. Could you give me some advice on how to start this project and what I would need? Maybe some materials would be helpful. Thank you in advance.