Need suggestion on generating PWM waveform
Hi All
I have a digital power converter topology (H-bridge) which requires waveform to look like the following:

As can be seen in the above, complementary waveform is being sent on bottom 2 channel in 1st 10ms and then they are being in the IDLE state while complementary waveform is being sent on other 2 channels in next 10ms.
I have achieved above using HRTIM (TIMERA and TIMERB) and TIM17.
The issue is that TIM17 interrupt the CPU and in the interrupt (in this case, at a freq. of 50hz), HRTIM outputs are being enable and disabled using the following code:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM16)
{
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
if(htim->Instance == TIM17)
{
static uint8_t toggle = 0;
toggle = !toggle;
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, toggle ? GPIO_PIN_SET : GPIO_PIN_RESET);
HAL_HRTIM_WaveformOutputStop(
&hhrtim1,
HRTIM_OUTPUT_TA2 + HRTIM_OUTPUT_TA1 + HRTIM_OUTPUT_TB2 + HRTIM_OUTPUT_TB1
);
HAL_HRTIM_SoftwareReset(&hhrtim1, toggle ? HRTIM_TIMERINDEX_TIMER_A : HRTIM_TIMERINDEX_TIMER_B);
HAL_HRTIM_WaveformOutputStart(
&hhrtim1,
toggle ? (HRTIM_OUTPUT_TA2 + HRTIM_OUTPUT_TA1) : (HRTIM_OUTPUT_TB2 + HRTIM_OUTPUT_TB1)
);
}
/* USER CODE END Callback 1 */
}
And this CPU intervention is something that I am trying to get rid of.
I would rather prefer to have hardware to generate the above waveform without CPU intervention. However, I have not been able to find any useful feature which would help me generate the above waveform (Closest is Burst Mode in HRTIM, but it applies burst to all the channel equally, which is not what I want). And this is where I need help!
Thanks