Skip to main content
Graduate
July 25, 2024
Question

Need suitable External Flash Loader - STM32F423ZHT6 GD25S512MDYIGR

  • July 25, 2024
  • 1 reply
  • 1065 views

Hi,

I'm creating a project on GUI using an embedded wizard. While I'm trying to flash the code to my STM32F423ZHT6 custom board. It shows an error: failed to erase memory.

I'm using STM32CubeProgrammer and I successfully erased the entire flash. But still it shows the same error. I'm using GD25S512MDYIGR QSPI Flash memory. So I need a suitable flash loader for the STM32CubeProgrammer.

Regards,

Meenakshi.

    This topic has been closed for replies.

    1 reply

    Graduate II
    July 25, 2024

    I can probably construct one, but would need the pin designations for the QSPI interface you have built.

    https://github.com/cturvey/stm32extldr/blob/main/README.md

    GD25S512MD