Question
Need to ignore the unwanted start bit during the stop mode.
I am working on STM32L051R8, which is set to use Stop mode, which wakes up on the start bit.
I have a situation where the MCU wakes up on an unwanted start bit, and UART extracts unwanted data. The expected action is to ignore the unwanted data and enable it to wake up again when it is supposed to.
I have tried to use
SET_BIT( huart1.Instance->CR1, USART_CR1_RE );
CLEAR_BIT( huart->Instance->CR1, USART_CR1_RE );
which kind of worked but when using below
CLEAR_BIT( huart->Instance->CR1, USART_CR1_RE ); the current consumption increased.