Nested interrupts on the Nucleo-F411RE
I am doing an academic activity where I was asked to execute a reading process from an external RTC via i2C, but on another MCU, I used a repeat timer, but I was unsuccessful. Something seems to interfere with the I2C communication and according to the analyzer (I am using a didactic simulator) the bus clock signal is not generated, but I see a series in the data signal exactly at the programmed time, so the firmware seems to freeze when writing to the I2C bus.
On an STM32 (especially on the Nucleo Nucleo-F411RE board) is it possible to nest the communication inside a repeat timer interrupt? I did not get to know in my studies on STM32 about which timers exist, which document should I read to learn more about this subject?