Question
No clock signal on SPI1_SCK
After configuring SPI1 in CubeMX and calling HAL_SPI_Transmit, I get a signal on the SPI1_MOSI line, but no signal on the SPI1_CK. I have confirmed that the pin is working correctly with other code and tried different clock speeds to see if that was the problem. Any ideas on why a clock signal is not being sent over SPI1_CK?