No device found on target error while dumping customized code for second time in STM32H735uC
Hi,
I have an application code(Call it as Code-1). I able to dump it into my custom STM32H735 board through ST-LINK V3 MINIE. But when i try to dump same code for second time, it showing below error,
" Target no device found"
Error in Initializing ST Link Device.
Reason: NO device found on target."
I have 2nd board, Field working code(Code-2). I Can able to dump this Code-2 into 2nd board multiple times. But when i tried to dump Code-1 into 2nd board, for first time i able to dump it. When i tried for 2nd time it showing same error as shown above.
I understand that the Code-1 modified SWD pin configurations(unintentionally), due to which second time ST Link is being not detected.
How to solve this problem?? Please suggest.
Thanks in advance,
Pavani