Skip to main content
Graduate II
January 24, 2025
Question

No error from null pointers

  • January 24, 2025
  • 3 replies
  • 1153 views

Hi,

I have been making a lot of calls into null pointers and am quite surprised at the results. I am expecting hard failures when I make this mistake but instead it seems that things just keep going and it takes a long time to realize I failed to initialize a pointer.

e.g.

LL_UCPD_RxEnable(Ports[PortNum].husbpd);

I have made this call which resolves to

#define SET_BIT(REG, BIT) ((REG) |= (BIT))
__STATIC_INLINE void LL_UCPD_RxEnable(UCPD_TypeDef *UCPDx)
{
 SET_BIT(UCPDx->CR, UCPD_CR_PHYRXEN);
}

I have made this with the value husbpd uninitialized. But nothing negative happens other than the operation doesn't complete. No crash or other error.

Is there anything I can do or enable that will produce a harder fault when I make this mistake?

    This topic has been closed for replies.

    3 replies

    Graduate II
    January 24, 2025

    There is memory mapped at ZERO, usually determined by the BOOTx pins

    Perhaps enable asserts() so the library sanity checks the pointers/parameters passed into the HAL upper layers.

    It will not help here, as it's not being checked.

    You could fill uninitialized memory with 0xCDCDCDCD type pattern, or something similar, that's more likely to throw a fault when used.

    Other Cortex-Mx parts you could perhaps play with watch points, or configure MPU to throw a MemManage_Handler

    Carl_GAuthor
    Graduate II
    January 25, 2025

    Thanks, ill look deeper. The pointers are all 0. So i guess its doing something there. Maybe I can put something at 0 to like the codes you suggested.

    Super User
    January 25, 2025

    You could use the Cortex-M memory protection unit:

    c - NULL pointer protection with ARM Cortex-M MPU - Stack Overflow

    After doing so, read/write access to the protected region(s) will raise the HardFault_Handler:

     

     /* Configure the MPU to prevent NULL-pointer dereferencing ... */
     MPU->RBAR = 0x0U /* base address (NULL) */
     | MPU_RBAR_VALID_Msk /* valid region */
     | (MPU_RBAR_REGION_Msk & 7U); /* region #7 */
     MPU->RASR = (7U << MPU_RASR_SIZE_Pos) /* 2^(7+1) region, see NOTE0 */
     | (0x0U << MPU_RASR_AP_Pos) /* no-access region */
     | MPU_RASR_ENABLE_Msk; /* region enable */
    
     MPU->CTRL = MPU_CTRL_PRIVDEFENA_Msk /* enable background region */
     | MPU_CTRL_ENABLE_Msk; /* enable the MPU */
     __ISB();
     __DSB();
    
     // ...
    
     *(int*)NULL = 0x1234; // triggers hard fault handler

     

    hth

    KnarfB