Not able to connect to STM32U5 Device from STlink debugger after programming Readout Protection level to 1
Hi ,
While exploring flashloader macro using IAR IDE to update Option bytes , I programmed FLASH_OPTR register with Readout Protection level 1.

Since then I am not able to communicate to device using STLink and following is the error

Is there anyway I can establish communication with device using debugger to rewrite the readout protection level bit to level 0. Please share your thoughts.
Regards,
Hareesha