nRF24L01+ receiver problems
Hello,
I am currently using a custom-built board designed to the nRF24L01+ specification and using the same exact circuit provided in their datasheet. It is connected to my STM32F103 through SPI. I am currently using this library to test out this board: https://github.com/elmot/nrf24l01-lib/tree/master
The board is able to successfully verify that it is connected to the NRF chip using the nRF24_Check() function. Furthermore, the nRF is returning back that a packet (without AA) has been sent successfully and subsequently clears the TX FIFO. On my receiver device, the RX FIFO does not get populated nor any interrupts triggered by the nRF which leads me to the assumption that there is a problem somewhere with the wireless transmission of the packet. If I were to enable AA, and also put my receiver device on the ESB RX example, then the nRF would return that the maximum number of transmissions has occurred.
It is my first time attempting to debug a wireless device that I have made so I would appreciate any help or suggestions on where to look and what to verify.