Nucleo-303RE Not Starting Up
I am using a Nuclro-303RE to develop a USB Virtual Com port, and I am running into an issue that I cannot seem to resolve. Just to verify things, I did put some really simple code in the flash the green indicator on the Nucleo board.
- I have it connected to a custom board that runs the USB lines out to a USB connector.
- It is powered externally with 5V to VIN. Jumper set for E5V. The power indicator on the Nucleo is on, and the 3.3V is running.
- I am able to run it with the debugger tool, however, it will not run with just the USB and the 5V in.
- When I plug in to the USB on the ST-Link board, it starts to run, i.e. the green LED will blink, and the USB will enumerate for the USB virtual com port.
- I did add an 8MHz oscillator @ X3 and associated parts.
- I do have a pull up on the USB line.