Skip to main content
Visitor II
July 16, 2025
Question

Nucleo-DRP1M1 with Nucleo-G0B1RE

  • July 16, 2025
  • 1 reply
  • 308 views

Im currently facing issues with DRP1M1 and the Nucleo-G0B1RE in source configuration.

I followed the instructions in the wiki however it seems that no actual communication is happening between the USB PD Devices this is the log i get from the cube monitor:

CAD 294121 0 USBPD_CAD_STATE_DETACH_SRC 0
EVENT 294121 0 EVENT_DETACHED 1
DEBUG 294122 0 VBUS OFF 2
DEBUG 294122 0 -- BSP_USBPD_PWR_VBUSOff -- 3
DEBUG 294154 0 ADVICE: USBPD_DPM_Notification:105 4
NOTIF 294154 0 USBSTACK_STOP 5
DEBUG 294154 0 ADVICE: USBPD_DPM_Notification:105 6
DEBUG 294154 0 -- BSP_USBPD_PWR_VBUSDeInit -- 7
DEBUG 294154 0 -- GDP/GDC setting : default -- 8
DEBUG 294154 0 -- BSP_USBPD_PWR_SetPowerMode -- 9
DEBUG 294154 0 -- Low Power -- 10
DEBUG 294154 0 -- BSP_USBPD_PWR_SetRole : SRC -- 11
CAD 294155 0 USBPD_CAD_STATE_DETACHED 12
CAD 294155 0 USBPD_CAD_STATE_EMC 13
DEBUG 299807 0 -- BSP_USBPD_PWR_VBUSInit -- 14
DEBUG 299807 0 -- BSP_USBPD_PWR_SetPowerMode -- 15
DEBUG 299807 0 -- Normal -- 16
CAD 299807 0 USBPD_CAD_STATE_ATTACHED_WAIT 17
CAD 299923 0 USBPD_CAD_STATE_ATTEMC 18
NOTIF 299923 0 USBSTACK_START 19
DEBUG 299923 0 ADVICE: USBPD_DPM_Notification:104 20
EVENT 299923 0 EVENT_ATTEMC 21
DEBUG 299923 0 VBUS ON 22
DEBUG 299923 0 -- BSP_USBPD_PWR_VBUSOn -- 23
DEBUG 299927 0 -- GDP/GDC setting : SRC -- 24
DEBUG 299927 0 ADVICE: USBPD_DPM_Notification:104 25
PE 299927 0 PE_SRC_STARTUP 26
NOTIF 299927 0 POWER_STATE_CHANGE 27
DEBUG 299927 0 ADVICE: USBPD_DPM_Notification:90 28
PE 299927 0 PE_SRC_SEND_CAPABILITIES 29
OUT 299929 0 SOP PD3 s:006 H:0x11A1 (id:0, DR:DFP, PR:SRC) SRC_CAPABILITIES DATA: 0A900100
Option:
[1] Fixed : 5V - 0.1A
30
OUT 299931 0 SOP PD3 s:006 H:0x11A1 (id:0, DR:DFP, PR:SRC) SRC_CAPABILITIES DATA: 0A900100
Option:
[1] Fixed : 5V - 0.1A
31
OUT 299932 0 SOP PD3 s:006 H:0x11A1 (id:0, DR:DFP, PR:SRC) SRC_CAPABILITIES DATA: 0A900100
Option:
[1] Fixed : 5V - 0.1A
32
PE 299934 0 PE_SRC_DISCOVERY 33

To me it looks like the source is detecting the sink but the sink is not able to repsond so the source times out and sends the capabilities multiple times. The cable i use is a marked cable and works fine with an USB-PD charger.

I tried debugging the issue for two days now but didnt find a solution. Simply using unmarked cables wouldn't work because our product must support a wide range of cables and adapters, so i didn't buy an unmarked cable for testing.

 

There was also an issue with the ADC and it stopped updateing when disconnecting the sink and reconnecting it again, since it tried to initialize the ADC even if it was still running.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 16, 2025

    Hi @PKrem.1 

    Would you please provide minimum software or attach your project. Otherwise, any supplementary information to help you dig deeper. 

    Technical Moderator
    August 15, 2025

    Hi @PKrem.1 

    I couldn't reproduce the issue on my Nucleo G071. I suggest you try to reproduce the behavior with the example provided here. It seems you didn't rely on TCPP configuration setup as provided. Please try to replicate the issue starting with the cube example provided to narrow down the issue and escalate to development team in case of any inconsistency.