Nucleo H723ZG, DEV_TARGET_HELD_UNDER_RESET
Hello community,
has anyone encountered DEV_TARGET_HELD_UNDER_RESET issues with a Nucleo Board (ST-Link V3) ?
I have multiple Nucleo H723ZG and for some reason I can't connect to any of them since a few days.
I have tried:
- swapping USB cables and adapters
- using a docking station or the notebook ports themselves
- external power supply vs. power supply over USB
- applying the board reset jumper and the ST-Link reset jumper
- trying to first power-up, then connect to computer
- the ST-Link Upgrade tool
- different IDE like VScode, STM32CubeIDE
- serial COM tools like Minicom
- turning off the computer and starting again
With all the combination I can max. achieve to see the board in the COM port (e.g. as /dev/tty.usbmodem21103), nothing more. Some boards draw 0.35A from remote which I find high, others only 0.1A. Others draw 500mA from the USB; which I find very high. It appears as if this is an issue with my computer...
STLINK-V3:
Product ID: 0x374e
Vendor ID: 0x0483 (STMicroelectronics)
Version: 1.00
Serial Number: 0018001C3156501520323443
Speed: Up to 480 Mb/s
Manufacturer: STMicroelectronics
Location ID: 0x01100000 / 1
Current Available (mA): 500
Current Required (mA): 500
Extra Operating Current (mA): 0
Any ideas?
Many thanks