NUCLEO H743ZI2 MB1364E and MB1364C
Hello, I hope you are doing great.
I have two NUCLEO H743ZI2, one of them is MB1364E, and the other one is MB1364C. They are totaly the same but there are little differences and I would like to find them and make them same, since I would like to use them in the same application.
I searched a lot and I found that there are some differences between them in the PCB and components.
For example,
1- SB1, 0 ohm 0603 resistor is deleted form the PCB in MB1364E.
2- SB45, a 0 ohm 0603 resistor is added to the PCB in MB1364E.
The question is that is there any other differences that I could not find?
Is there a PDF which explane the differences?
Best regards,