NUCLEO-H755ZIQ MCU went under low power state while debugging
I am using STM32s NUCLEO-H755ZIQ board , while debugging through eclipse IDE for the M7 core the board's MCU went under low power state and LD6 which is over current led (red) is turned on.
When I am connecting the board with the STM32CubeProgrammer the board is gettting detected but ST-Link is failing to flash the board.
Please help me with this problem as same thing has happend with the another NUCLEO-H755ZIQ board.
Both the boards are having same problem