Question
NVIC_PriorityGroupConfig() Undefined
Posted on February 26, 2016 at 03:02
The processor is an STM32F373VC using STM32CubeMX generated code with the FREERTOS option enabled.
I have attempted to add the code: NVIC_PriorityGroupConfig( NVIC_PRIORITYGROUP_4 ); to the code in main.c as instructed in the red text on page: http://www.freertos.org/RTOS-Cortex-M3-M4.html (I had to figure out the argument must have all capital characters). and as instructed in the comment in line 221 in the file ''stm32f3xx_hal_cortex.c''. I cannot find the function NVIC_PriorityGroupConfig() defined anywhere, nor can the gcc compiler running in Ac6. Where is it?