OB programming issue on the custom bootloader
Hello,
To protect the device's software, I am updating the RDP values in my own bootloader software, and to protect it in the event of a sudden power outage, I am also updating the BOR values. I am performing these updates only using HAL APIs. Additionally, I am writing the option bytes one by one. During development and testing, this worked flawlessly. However, the device has now entered serial production, and we are programming in large quantities. So far, 200 MCUs have been programmed, and approximately 50 of them ended up with an RDP value of 0xFF and the BOR value not set. I urgently need assistance regarding this issue. Production has been halted and is waiting for this problem to be resolved. Please help me.
I am adding the code block where I perform this operation below.
/* USER CODE BEGIN 2 */
#ifndef DEBUG
FLASH_OBProgramInitTypeDef ob_init;
// Unlock Flash and Option Bytes
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
// Get current configuration
HAL_FLASHEx_OBGetConfig(&ob_init);
// Check current RDP level
uint32_t curr_rdp_level = ob_init.RDPLevel;
// Only proceed if either BOR or RDP needs to be changed
if (OB_RDP_LEVEL_1 != curr_rdp_level)
{
if ((ob_init.USERConfig & OB_BOR_LEVEL_2) != OB_BOR_LEVEL_2)
{
ob_init.OptionType |= OPTIONBYTE_USER;
ob_init.USERType = OB_USER_BOR_LEV;
ob_init.USERConfig &= ~(FLASH_OPTR_BOR_LEV);
ob_init.USERConfig |= OB_BOR_LEVEL_2;
if (HAL_FLASHEx_OBProgram(&ob_init) != HAL_OK)
{
Error_Handler();
}
}
ob_init.OptionType = OPTIONBYTE_RDP;
// Configure RDP Level 1
ob_init.RDPLevel = OB_RDP_LEVEL_1;
// Program the option bytes
if (HAL_FLASHEx_OBProgram(&ob_init) != HAL_OK)
{
Error_Handler();
}
if (HAL_FLASH_OB_Launch() != HAL_OK)
{
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
Error_Handler();
}
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
HAL_Delay(100);
HAL_NVIC_SystemReset();
}
else
{
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
#endif