OCTO SPI output impedance on H7-series
I have swapped from a custom PCB-board with a 6-layer stack using a STM32H725IGKB, to another custom board with a 4-layer stack using STM32H723ZGT6 (simpler package).
I am using an external OCTO SPI on both boards, but I have R/W errors with the 4-layer board.
Both boards are routed with 50 ohms impedance and uses 33 ohms series resistors for the OCTO SPI.
I am wondering if the output impedance is the same for these two H7-devices?