OctoSPI Flash in memory mapped mode also used for application data
Hi,
We have a customer board with STM32H735 and OctoSPI flash in memory mapped mode.
Memory is used for TouchGfx elements and as external code memory.
Now we should add a simple file system for saving some data on the board.
Is it possible to use a file system (read/write access) on a OSPI flash in memory mapped mode.
Due to AN5050 and other resources i would say its not possible.
Can someone confirm to me if this is the case or if there is a way to solve this.