Skip to main content
Visitor II
December 26, 2025
Question

OCTOSPI signal integrity issue on STM32H723 vs STM32H725

  • December 26, 2025
  • 2 replies
  • 70 views

Hello everyone,

This is my first post on the ST Community forum.

I recently moved from a custom 6-layer board using STM32H725IGKB to a simpler 4-layer board using STM32H723ZGT6. Both designs use an external OCTOSPI memory, with 50 ohm controlled-impedance routing and 33 ohm series resistors on the signals.

On the new 4-layer board, I am seeing read/write errors on the OCTOSPI interface, while the original 6-layer board works reliably with similar routing and firmware.

I would like to ask whether the OCTOSPI output driver characteristics or output impedance differ between STM32H725 and STM32H723, or if these issues are more likely related to signal integrity, stack-up, or return-path differences on a 4-layer PCB.

Any guidance or experience would be appreciated.

Thank you in advance.

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    December 26, 2025

    Hello @Jonshill and welcome to the ST community,

    I think better to start to read this application note: AN4803 "High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs" and use IBIS information with HyperLynx tool and run simulations.

    JonshillAuthor
    Visitor II
    December 27, 2025

    Thanks for the suggestion. I’ll go through AN4803 and look into running IBIS-based simulations with the HyperLynx SI tool  to better understand the signal integrity aspects on this new board.

    Quick question: when using the HyperLynx tool with the STM32 IBIS models, are there any common pitfalls or specific settings you recommend for STM32H7 devices that I should pay attention to?

    Technical Moderator
    December 27, 2025

    Nothing special to STM32H7. That application note provides STM32F7 and STM32MP15 but as examples. STM32F7 as a microcontroller and STM32MP15 as a microprocessor. The same process should applies to STM32H7.

    If I answerd your original question please accept my previous post as solution.

    Thanks.