one bit is getting shifted at a particular byte in SPI Slave DMA mode in Stm32G0K6T6
Hello community ,
I have configured STM32G030 as SPI Slave in DMA mode where master commands poll rate at 50 ms . I have set NSS pin as Hardware input as it is slave .
As soon as NSS pin PB0 detects ,SPI DMA transmission starts in hardware level.
Payload length is 9 Bytes where last two bytes are dummy . sometimes one bit is in 7th byte's nibble(checksum) is getting left shifted by 1 . so checksum is getting failed .
example:- {0x44,0x00,0x00,0x11,0x00,0x00,0x8a,0x00,0x00,};(checksum should be 0x89 (1000 1001) ,but it is received as 0x8a(1000 1010))
kindly give your suggestions for solving this
SPI_HandleTypeDef spi_handle;
DMA_HandleTypeDef hdma_spi1_tx;
DMA_HandleTypeDef hdma_spi1_rx;
uint8_t hctrl_input_msg[10];
uint8_t hctrl_output_msg[10] ;
void HAL_SPI_MspInit(SPI_HandleTypeDef *hspi)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(hspi->Instance == MB_SPI)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
PB0 ------> SPI1_NSS
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF0_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF0_SPI1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* SPI1 DMA Init */
/* SPI1_RX Init */
hdma_spi1_rx.Instance = DMA1_Channel2;
hdma_spi1_rx.Init.Request = DMA_REQUEST_SPI1_RX;
hdma_spi1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi1_rx.Init.Priority = DMA_PRIORITY_HIGH;
if (HAL_DMA_Init(&hdma_spi1_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi1_rx);
/* SPI1_TX Init */
hdma_spi1_tx.Instance = DMA1_Channel3;
hdma_spi1_tx.Init.Request = DMA_REQUEST_SPI1_TX;
hdma_spi1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi1_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
if (HAL_DMA_Init(&hdma_spi1_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmatx,hdma_spi1_tx);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
void spi_slave_init(void)
{
spi_dma_enable();
/* Set the SPI parameters */
spi_handle.Instance = SPI1;
spi_handle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
spi_handle.Init.Direction = SPI_DIRECTION_2LINES;
spi_handle.Init.CLKPhase = SPI_PHASE_2EDGE;
spi_handle.Init.CLKPolarity = SPI_POLARITY_LOW;
spi_handle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
spi_handle.Init.CRCPolynomial = (uint32_t)7;
spi_handle.Init.DataSize = SPI_DATASIZE_8BIT;
spi_handle.Init.FirstBit = SPI_FIRSTBIT_MSB;
spi_handle.Init.NSS = SPI_NSS_HARD_INPUT;
spi_handle.Init.TIMode = SPI_TIMODE_DISABLE;
spi_handle.Init.Mode = SPI_MODE_SLAVE;
spi_handle.Init.NSSPMode = SPI_NSS_HARD_INPUT;
if (HAL_SPI_Init(&mb_spi_handle) != HAL_OK)
{
Error_Handler();
}
// set DMA TRANSMIT /RECEIVE source ,destination addressses
if(HAL_OK != HAL_SPI_TransmitReceive_DMA(&spi_handle,(uint8_t *)hctrl_output_msg,(uint8_t *)hctrl_input_msg,7))
{
Error_Handler();
}
}
static void spi_dma_enable(void)
{
__DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel2_3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel2_3_IRQn,0,0);
HAL_NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
}
/******************************************************************************/
/*! \brief Handles an NSS interrupt to prepare and terminate SPI transfers.
* \param void
* \return void
*******************************************************************************/
void EXTI0_1_IRQHandler()
{
__HAL_GPIO_EXTI_CLEAR_IT((uint32_t)GPIO_PIN_0);
}
//End of Transmission & Reception
void DMA1_Channel2_3_IRQHandler(void)
{
HAL_DMA_IRQHandler(&hdma_spi1_tx);
HAL_DMA_IRQHandler(&hdma_spi1_rx);
if((hdma_spi1_tx.ErrorCode == HAL_DMA_ERROR_NONE) && (hdma_spi1_rx.ErrorCode == HAL_DMA_ERROR_NONE))
{
notify_exchange_complete();
}
else
{
notify_exchange_fail();
}
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
hspi->State = HAL_SPI_STATE_READY;
}
void HAL_SPI_ErrorCallback(SPI_HandleTypeDef *hspi)
{
notify_exchange_fail();
}
Thanks
Narendra C