Skip to main content
Explorer II
October 15, 2024
Question

Option Bytes to RDB level 2

  • October 15, 2024
  • 1 reply
  • 2066 views

I am using Segger JLINK for software downloading to below boards. After downloading software, there is need to enable RDL level 2. Kindly give support below platforms.
STM32L562VET6

STM32L552VET6

STM32L552CCT6

Edit: I am using SEGGER J-Flash for software downloading. I need to understand wiki.segger.com/images/7/78/STM32L5_Lock.jflash and add my existing .jflash file.

Thanks

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 15, 2024

    Hello @gopikrishnan ,

    To enable RDP level 2 on STM32L5 series boards, you can follow these steps:

    1. Connect the Board to your computer via the Segger JLINK.
    2. Launch the STM32CubeProgrammer software.
    3. In STM32CubeProgrammer, connect to the target device using the JLINK interface.
    4. Once connected, go to the "Option Bytes" section in the STM32CubeProgrammer.
    5. Set RDP Level to 2 (select the value corresponding to level 2: "0xCC"), then click on "Apply" to set the RDP level to 2.

    How to regress from RDP level 2 to RDP level 0 on ... - STMicroelectronics Community

    Explorer II
    October 15, 2024

    Hi, I am using SEGGER J-flash. I am trying to understand how this will impact my current jflash with none of init and exit actions.
    wiki.segger.com/images/7/78/STM32L5_Lock.jflash

     

    Thanks,