OSPI as QSPI on L5 with W25Q256
I have a custom designed PCB board where I have used STM32L56 and W25Q256 along with other components. First, I was using SPI for interfacing but it was taking so much time when writing/reading MBs file. So I have to opt for QSPI now. L5 doesn't have specific QSPI, but using OSPI we can configure it as Quad SPI.
So, my questions are
1) what is difference between QSPI and OSPI as QSPI (command and working mechanism)
2) will this code work for OSPI as QSPI
3) if you have any test code for OSPI as QSPI, I can test and will modify it according to my needs
Looking forward to your response
Below are my configurations, code files with changes accordingly.
void testQSPI(){
OSPI_RegularCmdTypeDef s_command = {0};
/*uint8_t pData[3];
uint8_t wData[0x100];
uint8_t rData[0x100];*/
uint8_t pData[3];
uint8_t wData[0x100];
uint8_t rData[0x100];
memset(pData, 0x00, sizeof(pData));
memset(wData, 0x00, sizeof(wData));
memset(wData, 0x00, sizeof(wData));
uint32_t i;
printf("***************QuadSPi Example*******************************\r\n");
BSP_QSPI_Init();
BSP_QSPI_Erase_Chip();
/*##-2-Read Device ID Test ###########################################*/
/* Read Manufacture/Device ID */
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_ID_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = HAL_OSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
// s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(&hospi1, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("SPI I/0 Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Dual I/O*/
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = DUAL_READ_ID_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_2_LINES;
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_2_LINES;
s_command.AlternateBytesSize= HAL_OSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0;
s_command.DataMode = HAL_OSPI_DATA_2_LINES;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
// s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(&hospi1, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Dual I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Quad I/O*/
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = QUAD_READ_ID_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_4_LINES;
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_4_LINES;
s_command.AlternateBytesSize= HAL_OSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0x00;
s_command.DataMode = HAL_OSPI_DATA_4_LINES;
s_command.DummyCycles = 4;
s_command.NbData = 2;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
// s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(&hospi1, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Quad I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read JEDEC ID */
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_JEDEC_ID_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_NONE;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = HAL_OSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 3;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
// s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(&hospi1, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Read JEDEC ID : 0x%2X 0x%2X 0x%2X\r\n\r\n",pData[0],pData[1],pData[2]);
/*##-3-QSPI Erase/Write/Read Test ###########################################*/
/* fill buffer */
for(i =0;i<0x100;i ++)
{
wData[i] = i*2;
rData[i] = 0;
}
if(BSP_QSPI_Erase_Block(0) == QSPI_OK)
printf(" QSPI Erase Block ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Write(wData,0x00,0x100)== QSPI_OK)
printf(" QSPI Write ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Read(rData,0x00,0x100)== QSPI_OK)
printf(" QSPI Read ok\r\n\r\n");
else
Error_Handler();
printf("QSPI Read Data : \r\n");
for(i =0;i<0x100;i++)
printf("0x%02X ",rData[i]);
printf("\r\n\r\n");
for(i =0;i<0x100;i++)
if(rData[i] != wData[i])printf("0x%02X 0x%02X ",wData[i],rData[i]);
printf("\r\n\r\n");
/* check date */
if(memcmp(wData,rData,0x100) == 0 )
printf(" W25Q128FV QuadSPI Test OK\r\n");
else
printf(" W25Q128FV QuadSPI Test False\r\n");
}