Question
Output comparison pulse problem
On the stm32h750, I want to use 4 channels to implement pwm waves with different phases in the output comparison mode of tim8. Chanel's mode selection switches on match. The stages are 0% 25% 50% 75%. When the phase is zero (sConfigOC.Pulse = 1-1), the waveform does not flip, while other channels flip according to the set phase.