Skip to main content
Visitor II
July 29, 2025
Question

Overflow occurred when fetching Two encoder data

  • July 29, 2025
  • 1 reply
  • 454 views

We are working with the STM32 Nucleo-G474RE board and using two quadrature encoders—NEMA 23 and NEMA 34—connected through AM26LS32 line receivers to TIM2 and TIM3 respectively, configured in encoder mode. In our project, we initialized TIM2 and TIM3 with `CounterMode_UP`, no prescaler, and appropriate encoder mode settings. We initially tested with pull-down resistors and counter mode set to down, but encountered erratic behavior: encoder counts would overshoot, then suddenly reset to 0 or toggle between 0 and 1. We then tried changing the GPIO configuration to pull-up with counter mode set to up, but received no response from the encoders. Despite using `HAL_TIM_Encoder_Start()` and observing the encoder signals on an oscilloscope (which looked clean), the counter readings remained unstable or stuck. We are using the ITM SWV output to log values via printf. We would appreciate any insights or suggestions from the STM32 community on solving this encoder reading issue, especially in terms of correct GPIO configuration or timer settings for reliable quadrature decoding using the AM26LS32 with differential signal inputs.code is written below

 

/* USER CODE BEGIN Header */

/**

 ******************************************************************************

 * @file : main.c

 * @brief : Main program body

 ******************************************************************************

 * @attention

 *

 * Copyright (c) 2025 STMicroelectronics.

 * All rights reserved.

 *

 * This software is licensed under terms that can be found in the LICENSE file

 * in the root directory of this software component.

 * If no LICENSE file comes with this software, it is provided AS-IS.

 *

 ******************************************************************************

 */

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"

#include "stdio.h"



/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */



/* USER CODE END Includes */



/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */



/* USER CODE END PTD */



/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */



/* USER CODE END PD */



/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */



/* USER CODE END PM */



/* Private variables ---------------------------------------------------------*/



TIM_HandleTypeDef htim2;

TIM_HandleTypeDef htim3;



UART_HandleTypeDef huart2;



/* USER CODE BEGIN PV */



/* USER CODE END PV */



/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_USART2_UART_Init(void);

static void MX_TIM3_Init(void);

static void MX_TIM2_Init(void);

/* USER CODE BEGIN PFP */



/* USER CODE END PFP */



/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

int _write(int file, char *ptr, int len)

{

 int DataIdx;

 for (DataIdx = 0; DataIdx < len; DataIdx++)

 {

 ITM_SendChar((uint32_t)*ptr++);

 }

 return len;

}



/* USER CODE END 0 */



/**

 * @brief The application entry point.

 * @retval int

 */

int main(void)

{



 /* USER CODE BEGIN 1 */



 /* USER CODE END 1 */



 /* MCU Configuration--------------------------------------------------------*/



 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();



 /* USER CODE BEGIN Init */



 /* USER CODE END Init */



 /* Configure the system clock */

 SystemClock_Config();



 /* USER CODE BEGIN SysInit */



 /* USER CODE END SysInit */



 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_USART2_UART_Init();

 MX_TIM3_Init();

 MX_TIM2_Init();

 /* USER CODE BEGIN 2 */

 HAL_TIM_Encoder_Start(&htim2, TIM_CHANNEL_ALL);

 HAL_TIM_Encoder_Start(&htim3, TIM_CHANNEL_ALL);

 printf("STM32G474RE Encoder Reader - Started (via SWV ITM)!\r\n");

 printf("Manually turn the NEMA 23 shaft to see encoder count updates.\r\n");



 /* USER CODE END 2 */



 /* Initialize led */

 BSP_LED_Init(LED_GREEN);



 /* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/

 BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);



 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {



 /* USER CODE END WHILE */



 /* USER CODE BEGIN 3 */

 uint32_t current_encoder_count1 = __HAL_TIM_GET_COUNTER(&htim2);

 uint16_t current_encoder_count2 = __HAL_TIM_GET_COUNTER(&htim3);

 printf("Encoder Count1: %lu\r\n", current_encoder_count1);

 printf("Encoder Count2: %lu\r\n", current_encoder_count2);

 HAL_Delay(100);

 }

 /* USER CODE END 3 */

}



/**

 * @brief System Clock Configuration

 * @retval None

 */

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};



 /** Configure the main internal regulator output voltage

 */

 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);



 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4;

 RCC_OscInitStruct.PLL.PLLN = 85;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

 Error_Handler();

 }



 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;



 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)

 {

 Error_Handler();

 }

}



/**

 * @brief TIM2 Initialization Function

 * None

 * @retval None

 */

static void MX_TIM2_Init(void)

{



 /* USER CODE BEGIN TIM2_Init 0 */



 /* USER CODE END TIM2_Init 0 */



 TIM_Encoder_InitTypeDef sConfig = {0};

 TIM_MasterConfigTypeDef sMasterConfig = {0};



 /* USER CODE BEGIN TIM2_Init 1 */



 /* USER CODE END TIM2_Init 1 */

 htim2.Instance = TIM2;

 htim2.Init.Prescaler = 0;

 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim2.Init.Period = 4294967295;

 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;

 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;

 sConfig.IC1Filter = 0;

 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;

 sConfig.IC2Filter = 0;

 if (HAL_TIM_Encoder_Init(&htim2, &sConfig) != HAL_OK)

 {

 Error_Handler();

 }

 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)

 {

 Error_Handler();

 }

 /* USER CODE BEGIN TIM2_Init 2 */



 /* USER CODE END TIM2_Init 2 */



}



/**

 * @brief TIM3 Initialization Function

 * None

 * @retval None

 */

static void MX_TIM3_Init(void)

{



 /* USER CODE BEGIN TIM3_Init 0 */



 /* USER CODE END TIM3_Init 0 */



 TIM_Encoder_InitTypeDef sConfig = {0};

 TIM_MasterConfigTypeDef sMasterConfig = {0};



 /* USER CODE BEGIN TIM3_Init 1 */



 /* USER CODE END TIM3_Init 1 */

 htim3.Instance = TIM3;

 htim3.Init.Prescaler = 0;

 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim3.Init.Period = 65535;

 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;

 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;

 sConfig.IC1Filter = 0;

 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;

 sConfig.IC2Filter = 0;

 if (HAL_TIM_Encoder_Init(&htim3, &sConfig) != HAL_OK)

 {

 Error_Handler();

 }

 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)

 {

 Error_Handler();

 }

 /* USER CODE BEGIN TIM3_Init 2 */



 /* USER CODE END TIM3_Init 2 */



}



/**

 * @brief USART2 Initialization Function

 * None

 * @retval None

 */

static void MX_USART2_UART_Init(void)

{



 /* USER CODE BEGIN USART2_Init 0 */



 /* USER CODE END USART2_Init 0 */



 /* USER CODE BEGIN USART2_Init 1 */



 /* USER CODE END USART2_Init 1 */

 huart2.Instance = USART2;

 huart2.Init.BaudRate = 115200;

 huart2.Init.WordLength = UART_WORDLENGTH_8B;

 huart2.Init.StopBits = UART_STOPBITS_1;

 huart2.Init.Parity = UART_PARITY_NONE;

 huart2.Init.Mode = UART_MODE_TX_RX;

 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

 huart2.Init.OverSampling = UART_OVERSAMPLING_16;

 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

 huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;

 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

 if (HAL_UART_Init(&huart2) != HAL_OK)

 {

 Error_Handler();

 }

 if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)

 {

 Error_Handler();

 }

 if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)

 {

 Error_Handler();

 }

 if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)

 {

 Error_Handler();

 }

 /* USER CODE BEGIN USART2_Init 2 */



 /* USER CODE END USART2_Init 2 */



}



/**

 * @brief GPIO Initialization Function

 * None

 * @retval None

 */

static void MX_GPIO_Init(void)

{

 /* USER CODE BEGIN MX_GPIO_Init_1 */



 /* USER CODE END MX_GPIO_Init_1 */



 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOC_CLK_ENABLE();

 __HAL_RCC_GPIOF_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();

 __HAL_RCC_GPIOB_CLK_ENABLE();



 /* USER CODE BEGIN MX_GPIO_Init_2 */



 /* USER CODE END MX_GPIO_Init_2 */

}



/* USER CODE BEGIN 4 */



/* USER CODE END 4 */



/**

 * @brief This function is executed in case of error occurrence.

 * @retval None

 */

void Error_Handler(void)

{

 /* USER CODE BEGIN Error_Handler_Debug */

 /* User can add his own implementation to report the HAL error return state */

 __disable_irq();

 while (1)

 {

 }

 /* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

 * @brief Reports the name of the source file and the source line number

 * where the assert_param error has occurred.

 * file: pointer to the source file name

 * line: assert_param error line source number

 * @retval None

 */

void assert_failed(uint8_t *file, uint32_t line)

{

 /* USER CODE BEGIN 6 */

 /* User can add his own implementation to report the file name and line number,

 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

 /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

 

    This topic has been closed for replies.

    1 reply

    ST Employee
    August 26, 2025

    Hey @NasreenBanu

    The GPIO pins connected to the encoder signals should be configured as alternate function inputs, then the choice of pull-up or pull-down resistors depends on the encoder's output characteristics and the AM26LS32 line receiver