Skip to main content
Graduate
September 15, 2024
Solved

Perform fft on stm32f411

  • September 15, 2024
  • 1 reply
  • 1582 views

I am trying to make a music visualizer with led matrix and stm32f411 usb audio function
previously , i tried to use stm32f103 blue pill but the usb audio stuck and i can't find the reason

so i purchased the black pill to do it

 

but now the problem is the fft result is always drifted and seems not accurate

my usb audio  sample rate is 48k Hz

i have tried kissfft and  the fft in arm_math.h , they have similar result
for example ,when i play a 5k Hz sound on my pc , would result in peak at around 2.5kHz

and some similar peak at around 20kHz
i know that some fft result will have symmetric form at with start and end of the output buffer
but i think it is not the case

the video show i do some simple math to display the fft on led matrix from 0-20000Hz
the high frequency is at left , low frequency is at right

and you can see it kind of like being symmetric but not exactly ,especially the high frequency side is low at start

 

 

i am thinking of maybe the audio data have some problem
but i don't know how to verify

    This topic has been closed for replies.
    Best answer by uveuvenouve

    thank you
    i just realize that the data is in stereo
    and i have tested to print out one side of the the data

    when i play one side it have brunch of different data

    when i play other side it keeps printing 0 or 1

    it is quite match my expectation

     

    but when i feed the data to fft

    the result still strange and likely half of the played frequency

    and some strange frequency are rising as i observe

     

    however , i tested the almost same code this morning
    it run perfectly good....

    the possible reason i am thinking of is the uart ground was plugging to other pc at the first place

    1 reply

    Graduate
    September 15, 2024

    When you play a 5KHz tone, the FFT indicates a 2.5KHz tone - out by a factor of two (if you feed it 6KHz do you get 3KHz?). It is probably some simple error that is producing the factor 2 error. Perhaps try feeding the FFT with a simple mathematically(+timer) generated sine wave - ideally test the FFT with a standalone program, test each part of your program separately (eg. dump and check a portion of your ADC data when sampling the 5KHz tone). 

    uveuvenouveAuthorAnswer
    Graduate
    September 16, 2024

    thank you
    i just realize that the data is in stereo
    and i have tested to print out one side of the the data

    when i play one side it have brunch of different data

    when i play other side it keeps printing 0 or 1

    it is quite match my expectation

     

    but when i feed the data to fft

    the result still strange and likely half of the played frequency

    and some strange frequency are rising as i observe

     

    however , i tested the almost same code this morning
    it run perfectly good....

    the possible reason i am thinking of is the uart ground was plugging to other pc at the first place