Peripheral Clock Drift Tolerance on STM32F303ZE (USART, USB, SPI, I2C, ADC, CAN)
Hi ST community,
I'm using the STM32F303ZE in a design and need to ensure that the clocks for various peripherals stay within acceptable tolerances (in ppm or %) — especially across the full temperature range (–40°C to +105°C). I plan to use an external HSE crystal oscillator, and I’m trying to validate whether my chosen crystal (in terms of stability and accuracy) will meet the needs of the following peripherals.
Could you please help clarify the maximum allowable clock frequency drift for each of these peripherals:
USART (1–5)
What is the maximum clock drift (in % or ppm) tolerated between the transmitter and receiver over temperature?
How do oversampling modes (8x or 16x) and word length (M bits) affect this tolerance?
USB FS
I understand it requires 48 MHz ±0.25%. Is this tolerance strictly enforced by the USB hardware?
SPI (1–3)
For slave mode, is there a specified maximum allowable clock skew or drift from the external SPI master?
Are there any special considerations when using HSE as the SPI clock source, especially over temperature?
I2C (1–3)
For Fast-mode Plus (1 MHz), what is the acceptable clock inaccuracy or timing deviation for compliance?
Are there any temperature-related constraints defined by ST for reliable I2C operation?
CAN
What is the maximum oscillator tolerance (in % or ppm) per CAN node to ensure stable communication?
Is ±1% oscillator tolerance required per ISO 11898-1, or does ST recommend a more conservative value?