Skip to main content
Explorer
February 27, 2024
Solved

Pin PC13 in input mode with pull up option does not drive the pin high. STM32F411

  • February 27, 2024
  • 1 reply
  • 940 views

Hi,

I am trying to configure the pin PC13 in my STM32F411 device as Input with Pull up option and it is connected to a rotary encoder. At initial bootup time, the pin is in toggle state and after that, it is set to 0. In the same project, I also configured the RTC. This PC13 pin has an alternate function as RTC_AMP1, RTC_OUT, and RTC_TS. Could you please explain the reason for this?

Thanks and Regards

Vrinda R

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.

    Best Regards.

    STTwo-32 

    1 reply

    STTwo-32Answer
    Technical Moderator
    February 27, 2024

    Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.

    Best Regards.

    STTwo-32