Porting WICED sdk from STM32F423 to STM32U5A5
Good morning, I have to do a porting from a project developed on STM32F423 to an STM32U5A5
The starting project used the wiced sdk, with the supported platform STM32F423.
If I understand well, for STM32U5A the wiced sdk is deprecated, and it would be better to use the package Infineon.AIROC-Wi-Fi.Bluetooth-STM32. Is it correct?
Is there any application note to help me to do the porting? or to use the infineon package with STM32CubeMx?