Skip to main content
Graduate
December 3, 2024
Solved

Possible error in RM0444 REV_ID for STM32G071xx and STM32G081xx

  • December 3, 2024
  • 2 replies
  • 858 views

Hello everyone,

I wanted to ask if this is an error or if this is documented right:

When you take a look in the latest RM0444 Rev 5 reference manual on page 1373 there are the DBG registers explained. The "DBG device ID code register (DBG_IDCODE)"  for the STM32G071xx and STM32G081xx do have for the Revision Code Z and Revision Number 1.1 the REV_ID 0x1000. The same REV_ID is used for Revision code A and Revision number 1.0. I attached a screenshot of the manual.

Is this a typo or do they really have the same REV_ID for Revision code A and Z?

On the next page, the devices G031 and G041 are described, here with differing REV_ID`s. I think this should be the same for STM32G071xx.

Please let me know, if my assumption is true. And if this is not a typo, is there a way to find out what Revision number/code my G071 MCU does actually have?

Thanks in advance,

Michael

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello @MikeG ,

    Getting back to you as I had a feedback regarding your case and confirms that this is not a typo and RevA / RevZ have indeed the same REV ID value. In fact it was an exception for a internal manufacturing reasons.

    2 replies

    Technical Moderator
    December 3, 2024

    Hello @MikeG ,

    It will be escalated for verification. Internal ticket 197665 for tracking. I'll get back to you as soon as I have an answer.

    Thanks.

    mƎALLEmAnswer
    Technical Moderator
    December 4, 2024

    Hello @MikeG ,

    Getting back to you as I had a feedback regarding your case and confirms that this is not a typo and RevA / RevZ have indeed the same REV ID value. In fact it was an exception for a internal manufacturing reasons.