Possible issues when switching from UFBGA64 package to LQFP64 package.
Hello,
I am currently designing a product which uses the STM32G491REI6 (UFBGA64 package) as the PCB cost more because of the usage of micro and blind vias, i am thinking to switch to the LQFP64 package. I checked the datasheet https://www.st.com/resource/en/datasheet/stm32g491ce.pdf especially the 4.9 Pin definition section and it seems that both packages are compatible. I am asking the question now to confirm if both packages are fully compatible and if the only change required is a pin assignment change in the SW side. I would like to use LQFP64 as it will help me lower the cost. Could you support me in this issue?
Thank you.