Possible risks of voltage drop in VDD of STM32F3
Hi !
I am evaluating the risks associated with STM32F3, where I am speculating a case where the voltage drops in VDD for few microseconds. For an example, let us assume the voltage drops from 3.3V to 3.0V for few microseconds. This occurs every x ms (assume 1 or 10). Now, 3.0V is still a good range, but will this constant voltage drops lead to any risks over longer time? Any corruption in flash memory or weakening of protection diodes, etc..??
There are EMC related risks I understand from hardware perspective. What I am interested in is, the parts of controller that might be affected in the long run.
Thanks!