Skip to main content
Explorer II
May 19, 2025
Question

Possible to keep VDD33USB as NC if USB feature not using In STM32H753ZIT6

  • May 19, 2025
  • 1 reply
  • 347 views

Can we  keep VDD33USB keep NC if USB feature not using In STM32H753ZIT6?

If kept NC what may go wrong? 

    This topic has been closed for replies.

    1 reply

    Super User
    May 19, 2025

    NC is usually not the best idea , with any digital input pin;

    see ds :

    AScha3_0-1747636316782.png

    So you could leave it to gnd. But why not set it to vdd ? So later, if you want USB, its there.

    Explorer II
    May 19, 2025

    thanks @AScha.3 , I agree on this, I fact i suggested to keep zero ohm and tie it with VDD( 3.3V). but issue is we are in final stage of Gerber generation ( keept this pin NC) . Now need strong reason to modify it now. 

    also will you check on below snap?

    abhilash72_0-1747637224639.png

    if not used 0v to 3.6V. I not sure if 0V to 3.6V means not we can keep it NC.

    adding link of application note 

    *Getting started with STM32H723/733, STM32H725/735 and STM32H730 Value Line hardware development -

    FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

    Super User
    May 19, 2025

    From ds , 0...3v6 allowed, NC should be no problem for function of cpu.

    But as always: a floating input (here power input) is not the "perfect" design idea.