Power consumption of 6K vs. 12K SRAM in STM32C011F6 vs. STM32C031F6
Hello,
We are using the STM32C0 in a low-power application. We initially selected the part with 12K SRAM in case we needed to use more than 6K, but after development have found that we can make do with 6K. I am curious if there is any power savings by moving to the 6K part. The "Supply Current Characteristics" in the C011 vs C031 data sheets are cut-and-paste identical which leads me to believe that the extra SRAM has no impact on power consumption, in which case we would just stay with the 12K part. However, if the copy/paste was somehow an oversight and we could save some power by switching to the 6K part then we'd consider doing that.
Thanks,
TG