print messages are not coming in teraterm
Hai,
I am using STM32L496ZG-P board and STM32CUBE IDE (1.15.1).
I tried to print hello world in tera term using UART/USART,USB etc , i tried many programs by reffering many videos in youtube, and some docs from STM communinty link etc etc,. Maximum all the ways i tried , but running is successfull, i can debug also , but prints are not coming in tera term. Some basic baudrate ,stopbit etc settings are all i checked properly, still i am not getting.
Please help me for this.
I connected the STM32L496ZG-P board to the laptop using USB cable which is present at debugger side of the board. So is there any jumper settings or shall i have to use any usb converter or any tx rx pin i need to connect. Please tell me.
Thanku