Problem with st-flash while programming Nucleo H563ZI
I am using st-flash version of 1.8.0 to flash the binary into Nucleo H563ZI. In this process i have used erase command "st-flash --connect-under-reset erase" to check whether the hardware works or not. For the erase command i got below error
"
st-flash 1.8.0
2024-07-31T16:31:55 WARN common.c: NRST is not connected
2024-07-31T16:31:55 ERROR common.c: Soft reset failed: error write to AIRCR
2024-07-31T16:31:55 ERROR common.c: Can not connect to target. Please use 'connect under reset' and try again
Failed to connect to target
Failed to parse flash type or unrecognized flash type
"
I have also tried with st-link's git upstream master(1.8.0-39-gd7103ff) for testing yet the above error persists. I am using WSL2 on native windows machine.
Does anyone has similarish or related issues for the STM32H563ZI target?