Programming a virgin STM32G0B1
I'm trying to program a virgin SYM32G0B1 with the code I've developed and successfully run on the NUCLEO-G0B1RE/NUG0B1RE$AU2 development board. I'm using the STM32CibeProgrammer 2.20.0 software and an FTDI cable (TTL-232RG-VIP-WE with the Vcc line connected to the 3.3 Vdc rail) connected to LPUART1 on port PC0/PC1. I have the BOOT0 signal (PA14) tied to ground.
Having no success with my new hardware, I decided to try the development kit as a sanity check, so changed JP2 to use E5V and connected a 5-volt supply. The dev board runs just fine with that. I connected the FTDI cable to PC0/PC1 on CN10, and shorted PA14 on CN7 to ground. Unfortunately, I also cannot program that MCU. The programmer's log shows:
16:41:26 : RTS low
16:41:26 : DTR Low
16:41:26 : Serial Port COM6 is successfully opened.
16:41:26 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
16:41:30 : Timeout error occured while waiting for acknowledgement.
16:41:30 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
I've verified the FTDI cable works (short TX to RX and look for echoed characters) and swapped Tx with Rx, just in case that was the culprit.
I'm sure I must have overlooked something, but what?