Programming STM32U031C8U6 with ST-LinkV3
Good morning,
I would like to request support regarding the programming and debugging of the STM32U031C8U6 microcontroller. It is mounted on a custom-designed board, and I am experiencing issues connecting to the microcontroller via SWD for programming and/or debugging using an ST-LinkV3 updated to the latest version (V3.J16.M8.B5.S1), with STM32CubeProgrammer and STM32CubeIDE. The microcontroller is never detected.
Note: With the ST-LinkV2 programmer, I am able to perform both programming and debugging without issues using the same software tools.
Many thanks in advance to anyone who can help me!