Skip to main content
Visitor II
August 10, 2025
Question

Protection of SWD lines :: STM32L011

  • August 10, 2025
  • 1 reply
  • 276 views

Hello,

Is it recommended to implement an ESD protection on SWD lines of STM32L011D3/D4 mCU? I went through "Getting started with STM32L0xx hardware development" document and there is a Figure 15 which suggests to connect SWD lines direct to programming connector without any protections. I'm just thinking that some protection would be good, like 47R - 100R resistors on the lines with 3.3 V (or 5 V ?) Vrwm of ESD diodes while programmer would not be connected to the board?

Many thanks.

    This topic has been closed for replies.

    1 reply

    Super User
    August 10, 2025

    If you want more ESD protection that the chip already provides, you can add additional ESD diodes:

    TDK_0-1754832428810.png