PTP/USB controlling camera (STM32F4)
Hi,
I'm working on a project which should communicate with a camera (canon, Nikon ....) and should be able to get pictures from the camera through Usb port.
i search in the net for a way to do that and i found that the picture transfer protocol (PTP) is used for this purpose.
i have an STM32F4 Discovery board which include USB OTG connector and a Canon PowerShot SD3500 IS camera which should support the PTP protocol according to the
https://support.usa.canon.com/kb/index?page=content&id=ART126085
.So my questions are :
1/ I want to know if the STM32F4 Discovery board is able to get pictures from the camera using the PTP protocol
?
2/ Is there any library or example to help me to figure out how to do that or even how to start the project ?
3/ Should i get an OTG cable to connect it to my camera ?
4/ Can i even go further and not just limit the project to get picture but even control the camera, like send an order to take a shot .... similar to the
https://www.youtube.com/watch?v=aGAHeJVDePk
.any help is greatly appreciated,
regards,