Skip to main content
Visitor II
April 3, 2024
Question

Putting STM32L452 Sleep Mode

  • April 3, 2024
  • 1 reply
  • 621 views

I'm developing a board with an STM32L452 and would like to find out if I can low the power consumption.
The current draining is 35mA, my goal is lower it to 20mA or less to achieve a requirement.
I've tried putting the device to sleep putting SLEEP MODE or STOP 1 MODE using the followings code:

while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

 HAL_Delay(1000);
 HAL_SuspendTick();
 HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON,PWR_SLEEPENTRY_WFI);
 HAL_ResumeTick();

}

or

while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

 HAL_Delay(1000);
 HAL_SuspendTick();
 HAL_PWREx_EnterSTOP0Mode(PWR_SLEEPENTRY_WFI);
 HAL_ResumeTick();
}
/* USER CODE END 3 */

But I can not see any change in my current. Still Draining 35mA.
Any help would be appreciate it.

    This topic has been closed for replies.

    1 reply

    ST Employee
    April 4, 2024

    Hello @jkfc95, welcome to ST Community 

    With these values, I believe you're not successfully entering Sleep/stop0 mode at all. 

    As the expected Idd value in sleep mode is around 0.83mA and decreases when increasing Fhclk.

    Could you please describe more the conditions (Fhclk clocking, peripherals enabled, RTC disabled/enabled, WKUP source, debug on?) 

    Also, check this wiki article