Putting two 32-bit words in TxFIFO. How to guarantee USB controller doesn't send only half my data?
If my data is more than one 32-bit word and I have to write it one 32-bit word at a time to the FIFO, is it possible that the USB controller could send just the first 32-bit word? Is there a way to stop that from happening?
Thanks
```
USBx_DFIFO(1) = send.u32[0];
// Is it possible for the USB controller to send just the first 32bit word if timing is right?
USBx_DFIFO(1) = send.u32[1];
```