PWM jitter
Hello,
I am currently in the midst of developing a super simple system to create a varying load. It's basically to resistors in series with a transistor in parallel of the second resistor. The transistor is driven by a PWM signal to bypass the second resistor and modify the load.
I've been trying the circuit with a function generator and it's working perfectly.
I now need to switch the PWM generation to a timer of a STM32. I have a nucleog474RE.
I used one of the example code available via cubeIDE (TIM_PWMOutput) and changed the frequency to match what i need (3.2kHz) but whenever I try and use my circuit with it, the signal generated by the nucleo is nowhere near clean and smooth, there is a huge jitter that basically renders my circuit useless (I need very high precision and stability).
Would any one have any idea why this is happening and what to do to correct it ?
Thanks for the answers !