PWM problems
Hello! Recently I got into STM programming for my internship and I cannot figure out register level programming yet, I have this piece of code
```
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN | RCC_APB1ENR_TIM2EN;
GPIOA->MODER |=GPIO_MODER_MODE5_1 | GPIO_MODER_MODE5_0;
TIM2->CCER|=TIM_CCER_CC1E;
TIM2->CR1 |=TIM_CR1_ARPE;
TIM2->CCMR1 |=TIM_CCMR1_OC1M_1|TIM_CCMR1_OC1M_1|TIM_CCMR1_OC1M_0|TIM_CCMR1_OC1PE;
TIM2->PSC=42; //trivial
TIM2->ARR=1000; //trivial values
TIM2->CCR1=250; //trivial
TIM2->EGR |=TIM_EGR_UG;
TIM2->CR1 |=TIM_CR1_CEN;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
```
Which in theory, to me, looks like it should work, however there are things I still do not fully understand, for example: Here I wanted to use Tim2 on channel 1 because I can use that on my PA5 pin which is LED2 on my Nucleo f401RE board, and I wanted to produce a PWM signal on it, however, it just doesn't display, if someone could provide some feedback or guidance it would be greatly appreciated.