QSPI Data Transfer between MCU and FPGA
I have designed a PCB that connects an Artix-7 XC7A35T-1FTG256C FPGA with an STM32F469VET6 (LQFP 100) MCU. My goal is to transfer data between these two devices, with the MCU as the QUADSPI master and the FPGA as the slave. For communication, all QUADSPI pins of the MCU are connected to the FPGA. I need to perform periodic data transfers every 10 microseconds. Specifically, the FPGA should send 10 16-bit values to the MCU, which will process them and then send back 10 16-bit values to the FPGA.
As a starting point, consider sending 10 16-bit data to the FPGA, and reading 10 16-bit data from the FPGA. To ensure periodic transfers, I initially used a TIM2 interrupt, triggering every 10 microseconds. However, I am facing difficulties in performing both read and write operations reliably.
Most available references use QUADSPI in polling mode, which is blocking and unsuitable for my high-speed application. I want to use DMA to accelerate the process. Could you guide me on how to set up periodic QUADSPI transfers using DMA, ideally with an example where data transfer occurs every 10 microseconds?